04.06.2024
Webinaraufzeichnung
Englisch

IoT Sensors powered by Energy Harvesting

Inhalte, die Ihnen auch gefallen könnten

Energy Harvesting – our main topics during the webinar include:

  • An introduction to Energy Harvesting. What type of ambient energies are available?
  • Challenges in converting and storing these energies into usable energy
  • Examples of real life use. Cases demonstrating that Energy Harvesting progressing from the laboratory to commercial applications, as well as some power electronics-related applications for Energy Harvesting.
  • Converting the ambient energy to usable energy. How can sporadic problems with energy and voltage levels be solved? 
  • How much of the stored energy can be lost through leakage. Which tools/evaluation kits are available to develop self-powered electronics?
  • Discussing about low power converter IC’s, which can be powered from multiple harvesters at the same time, and manage the energy to power extreme low power microprocessors. These low power microprocessors have RF modules built in, can communicate wirelessly, and could be power completely autonomously.
  • Low power sensors

 

Presentation IoT Sensors powered by Energy Harvesting

Teilen auf:

Videos, die Ihnen auch gefallen könnten