19.03.2025
Webinaraufzeichnung
Englisch

Webinar Würth Elektronik PCBs: New UL listing for RIGID.flex: maximum performance - highest safety

Inhalte, die Ihnen auch gefallen könnten

Our RIGID.flex PCBs have long been established in all industries where miniaturization, maximum reliability and extreme requirements are needed - from medical technology and the automotive industry to aerospace. UL-listed for over 20 years, they now even meet the extended requirements of Underwriters Laboratories (UL) and comply with the strict North American safety standards.

This means: safe use worldwide - not just in the USA and Canada. Thanks to tested quality and simplified listing, RIGID.flex PCBs from Würth Elektronik are the ideal choice for UL-approved end products - whether in safety-critical industries or in aerospace, where extreme conditions prevail.

In our webinar we offer insights into:

  • UL basic knowledge:
    • Types of UL listing and their advantages
    • Which parameters and processes are defined with a UL type?
    •  Contents, rules and options of the UL marking
  • Temperature load, solder limits and soldering processes
  • How do I specify UL requirements correctly?
  • Consequences of using the wrong PCBs
  • What improvements does the new UL listing bring?

 

Webinar presentation

Teilen auf:

Inhalte, die Ihnen auch gefallen könnten