Stay Connected
Waldenburg (Germany), January 19, 2023 – Würth Elektronik now presents its “Electromechanical Components 2023” catalog to download. The catalog contains 65 pages with innovations from the areas of connection and assembly technology as well as switches and buttons. The manufacturer dedicates a chapter to the REDCUBE high-power contacts. Thanks to press-fit technology, they are particularly robust and vibration-resistant. All products in the catalog can be ordered from stock without a minimum order quantity. Developers can receive free samples on request.
The new catalog clearly shows the various options for connecting PCBs with one another or with cables. A highlight in the 2023 catalog is the M12 circular connectors with screw locking and IP67 or IP68 protection for data lines in industrial automation equipment. The coaxial connectors also include an interesting new arrival: various N-type coaxial connectors to the MIL-STD-348 standard for particularly rugged applications. Among the switches, a new toggle switch family catches the eye—with a current carrying capacity of 1 A, rated voltage of 30 V and ESD compliance with IEC 61000-4-2.
REDFIT CRIMP is a particularly stable yet reversible connection for up to 16 A and 400 V. This PCB connector uses Würth Elektronik patented SKEDD technology. A positioning pin allows non-rotating connection to the PCB by hand and without a mating connector.
The printed version of the catalog can also be ordered at:
https://www.we-online.com/en/products/components/service/information-components
Components
Components
Würth Elektronik expands its range of digital isolators
Continue Reading
Components
Components
25 June 2024: WE-DAY 2024 at MotionLab.Berlin
Continue Reading
Components
Components
Würth Elektronik presents its revised “Trilogy of Wireless Power Transfer”
Continue Reading