IQD extends Range of -40 to 125 °C crystals
Waldenburg (Germany), May 4, 2023 – Components capable of withstanding high operating temperatures are increasingly in demand, and it is not just by engineers working on the traditional high temperature or extreme applications, for example downhole. This trend is partly driven by IC manufacturers, who often design one chipset suitable for both industrial and automotive applications, and by the increased use of electronic devices in more extreme environments. Additionally, the internal self-heating of electronic components close to the crystal on the board can be a motivation to select a crystal that is guaranteed to operate within the specification up to 125 °C.
Customers who are using the same frequencies in multiple projects with different temperature requirements, may also benefit from selecting one extended temperature part that is designed to work within all these applications rather than having to source and stock multiple parts.
IQD is therefore introducing a range of crystals housed in the popular 4-pad SMD ceramic packages 3.2 x 2.5 mm (CFPX-180) and 2.0 x 1.6 mm (IQXC-42) with the extended operating temperature range of -40 to 125 °C. The CFPX-180 is available in a range of frequencies from 12.0 MHz and the IQXC-42 from 16.0 MHz, with various load capacitances. The parts are offered with frequency stabilities down to +-30ppm over -40 to 125 °C and the ESR values are specified slightly lower than for the existing range of crystals in order to meet the demands of new microcontrollers, which often require lower ESR, for example for IoT applications. For engineers requiring AEC-Q200 qualification, IQD also has a range of automotive qualified crystals. For a full list of the available frequencies and specifications please visit our website www.iqdfrequencyproducts.com.
These parts are recommended for multiple applications, including Internet of Things (IoT and IIoT), e.g.: