Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

27. June 2024
Components

2-Channel Digital Isolators now with 5000 V Isolation Voltage

Content you may also like

Two 2-Channel Digital Isolators

Würth Elektronik is expanding its portfolio of digital isolators with a two-channel version in SOIC 8WB package (5.85 x 11.5 x 2.8 mm). The new design boasts an isolation voltage of 5 kVRMS. This is particularly important for electronic devices operating in environments exposed to high voltages and EMC interference which need 2-channel digital isolators with high isolation voltage. The isolators are ideally suited for high-speed applications up to a data rate of 150 Mbps and are characterized by their high common mode transient immunity (CMTI) to system noise of ±150 kV/µs.

SMT-mountable digital isolators are used for galvanic isolation in transmitting digital signals. This ensures reliable data transmission without distortion or errors to protect people or sensitive circuits from high voltage. The WPME-CDIS (Capacitive Digital Isolator Standard) series of isolators with UL 1577 approval can be used, for example, in test and measurement systems, battery management systems, solar inverters, industrial switching power supplies and motor controllers as well as for isolating communication buses. Alongside the new components, there are already various two-channel and four-channel configurations with high or low default output. With its designation WPME-CDIP (Capacitive Digital Isolator Powered), Würth Elektronik also offers capacitive digital isolators with integrated DC/DC converter.

Free samples of all the digital isolators can be ordered from Würth Elektronik.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in