On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik extends its terminal block connector series
Waldenburg (Germany), November 28, 2023 – Würth Elektronik is extending its WR-TBL series by screwless push-in connectors in the 3.5mm and 3.81mm pitches. The new 4101, 8101, 4093, and 8093 series come close to matching the specifications of the screw-fixed connectors and can replace them. Another important feature for customers with SMT-dominated production lines: The THR series 8101 and 8093 are designed for soldering in the reflow oven.
The housing of the connectors in the THR series is made of a high-temperature plastic, the pins are shorter in length, and the connectors are supplied in automatically processable belt format. The 4101 (THT) and 8101 (THR) series in the 3.5mm pitch are available with horizontal, vertical, and 45° cable entries. The 4093 (THT) and 8093 (THR) series in the 3.81mm pitch have a 45° cable entry.
The terminal blocks are available from stock with two to twelve pins. 13- to 24-pin connectors can be supplied on request as per customer specifications.
All the series named above have both cULus and VDE certification.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press Information and pictures of the company area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik Blog
Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.