Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

04. September 2024
Components

Reproducible Transmission Quality for High-Frequency Lines

Content you may also like

WR-SMA

Würth Elektronik presents its solderless coaxial sockets

Würth Elektronik expands its SMA connector family for high-frequency applications to include WR-SMA PCB Solderless. The solderless approach allows quick and easy assembly without damage to the PCB. Besides simplifying the installation process, which requires no soldering equipment, the solderless SMA connectors can be reused multiple times, making them suitable for prototyping or temporary use. This makes them an affordable solution for efficient testing. What’s the biggest advantage of these sockets? Because no solder is required on the signal pin, reproducible connection quality is achieved, and impedance variation due to the amount of solder paste is avoided.

Würth Elektronik has opted to use brass instead of stainless steel for its connector family, which differs from many of its competitors by providing a cost advantage while maintaining the same electrical performance. The screwed clamp connector provides a highly robust mechanical connection. Additionally, the solderless coax connectors allow for easy repairs and hassle-free replacement in the field, without the need for special tools or knowledge. The SMA sockets are suitable for both strip and multistrip lines, as well as coplanar waveguides.

As the SMA interface complies with the MIL-STD-348 standard, is designed for 50 ohms, and supports up to 27 GHz, the solderless coax connectors are particularly suitable for high-frequency PCB applications that require precision. The connectors are recommended for test equipment, for evaluation boards, and for applications with an operating temperature range from -65°C to +165°C.

Developers looking to use these connectors in telecommunications, broadband, and antenna-related wireless applications or testing equipment can obtain free samples from Würth Elektronik.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in