Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

11. January 2022
Intelligent Systems

Plug Instead of Screw – Completely Lead-Free

Content you may also like

Kampagnenbild der bleifreien Powerelemente LF PowerBasket SMD

The Inventor of Powerelements Expands Its Portfolio of Lead-Free High Current Contacts

The LF PowerBasket SMD series from Würth Elektronik ICS offers lead-free Powerelements for pluggable contacting on printed circuit boards. A new bushing variant with a diameter of 6 mm has recently been added to the company’s portfolio.

PowerBasket SMD High Current Contacts are the result of the progress has been made in consistently developing our pluggable LF PowerBasket products in line with market requirements. The Powerelements of this product series are designed to reduce the effort required to assemble components. The LF PowerBasket SMD Power Supply Terminals are multi-pluggable and are ideal for use in wire-to-board and board-to-board connections. Compared to conventional systems, the special design of the contact blades significantly reduces the insertion and extraction forces. Due to the high position tolerance of up to 0.6 mm, several contacts can be plugged in at the same time. This offers a considerable advantage for three-phase connections, for example.

The Powerelements feature a high current carrying capacity of up to 160 A at 20 °C. A special alloy makes it possible to use them at higher ambient temperatures. Depending on the design, the operating temperature range can be up to 150 °C and even up to 170 °C for short periods.

LF PowerBasket Powerelements can be processed in conventional SMT lines and are soldered in a convection oven or via a vapour phase system. They are supplied on a reel in ESD blister packaging, optionally with Kapton sticker. This enables fast and cost-effective assembly.

The LF PowerBasket SMD High Current Contacts are produced using a punching and bending process and can therefore be manufactured without any lead additive. They are totally lead-free and RoHS compliant - and thus completely unaffected by the possibly soon expiring exemption 6c of the RoHS Directive, which allows four percent lead in copper alloys for electrical and electronic equipment. To ensure a greater degree of planning reliability, manufacturers should monitor their project development times and product life cycles that stretch over several years and switch to lead-free solutions in time. Würth Elektronik ICS is one of the first companies on the market to also offer its High Current Contact portfolio as a lead-free variant (LF Powerelements). Customers and interested parties can find all the information they need on the subject ‘lead-free’ on the online platform LF-Powerelements.com.

Lead-free LF PowerBasket Powerelements series for pluggable contacting on printed circuit boards in SMD 3 mm and SMD 6 mm versions

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in