On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik expands its series of signal transformers for large energy storage devices and UPS
Waldenburg (Germany), April 9, 2024 – Würth Elektronik expands its WE-BMS transformer series for battery management systems with versions for an operating voltage of 1500 VDC. The component design features enhanced isolation in line with IEC 62368-1 with triple-insulated wire (primary and secondary side), as well as galvanic isolation and a test voltage of 6400 VDC. All this makes the new models in the series ideal for use in large stationary energy storage systems from solar and wind farms, in intermediate storage systems in high-power charging stations to balance out peak loads, or for uninterruptible power supplies used in critical infrastructures.
Battery management systems ensure safe operation of battery packs and provide information on battery and charge status. The downstream BMS controllers are connected in series, as are the battery cells. As voltage differences and electromagnetic interference can arise between the components connected in series, a BMS transformer helps isolate the components from each other and suppress interference. The latest members of Würth Elektronik's BMS transformer series guarantee this, even in systems with a high operating voltage of up to 1500 VDC. The longevity of the enhanced isolation of the modules as defined in IEC 62368-1 was tested using the partial discharge test in accordance with IEC 60664-1.
The transformers for battery management systems are now available from stock without a minimum order quantity.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press Information and pictures of the company area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik Blog
Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.