Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

23. March 2023
Components

Switch On, Over and Off

Content you may also like

Drei Bauelemente liegen auf einer weißen Fläche. Das Mittelteil ist rot und ein Ende des Teils ist ein Schalter.

Würth Elektronik introduces its toggle switch family

Waldenburg (Germany), March 23, 2023 – Würth Elektronik now also produces high-quality toggle switches. Different versions of the user-friendly fast switches are now available under the name WS-TOTV. The switches are ESD compliant to IEC 61000-4-2 and have undergone operating endurance testing under full load to prove their durability (electrical life: 50,000 steps).

Toggle switches are commonly used to switch between functions on devices, which is why Würth Elektronik offers them with both ON/OFF/ON and ON/ON switching functions. They are available for SPDT (Single Pole Double Throw) and DPDT (Double Pole Double Throw) schematics as well as in horizontal and vertical versions. Their current carrying capacity is 1 A at a rated voltage of 30 V. The withstanding voltage extends to 500 V and the operating temperature from -40 up to +85°C. The frame complies with flammability class UL94 V-0.

Options include a locking ring as mechanical anti-twist protection for assembly in the 6.35 mm panel cutout, and caps in red or black. Würth Elektronik also supplies caps in any color for larger orders. Free samples for developers can now be ordered.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in