On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik introduces its WCAP-FTDB DC-Link capacitors
Waldenburg (Germany), March 30, 2023 – Würth Elektronik presents a new series of film capacitors specially designed for DC-Link applications. The WCAP-FTDB series components can be used in the voltage range from 500 to 1200 V and are characterized by high ripple current capability. This makes them particularly attractive for use in AC/DC and DC/DC converters for charging systems and power electronics in e-mobility or in renewable energy solutions. The 24-model product family offers capacitance values from 1 µF to 75 µF.
The capacitors for stabilizing DC-Link voltage are very robust. Thanks to their metallized polypropylene film design, they have self-healing properties whereby short circuits “burn out” their own cause, hence restoring an intact dielectric. Significantly more durable than other capacitor types, the WCAP-FTDB series is suitable for applications with long maintenance cycles like wind turbines. Würth Elektronik provides a boxed THT package with pitch of 27.5 mm, 37.5 mm and 52.5 mm for this component family. The operating temperature of the film capacitors extends from -40°C to 105°C, the respective maximum voltage values attained are up to 85°C.
Like all products in the Electronic Components 2022/2023 catalog, the WCAP-FTDB DC-Link capacitors are now available without a minimum order quantity. Würth Elektronik provides free samples and offers a wide range of characteristic measurement data of the capacitors in the REDEXPERT online tool. This facilitates the selection of suitable components.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press Information and pictures of the company area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik Blog
Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.