Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

25. March 2025
Components

EMC Protection – Now Also Available for Thin Cables

Content you may also like

WE-STAR-TEC, the well-known snap ferrites from Würth Elektronik, are now also available for cables with a diameter of just 2 to 3 mm.

Würth Elektronik expands its STAR-TEC and STAR-TEC LFS snap ferrite families

Snap ferrites, developed in-house with technology using keys for retroactive cable noise suppression, are among the products that have made Würth Elektronik so well-known. The STAR‑TEC and STAR-TEC LFS product families have since grown: There is now a ferrite available for cable diameters of 2 to 3 mm that features all the proven practical benefits familiar from Würth Elektronik snap ferrites.

EMC protection is becoming increasingly important for applications using smaller cable diameters as compact packages are facing more sources of interference. This makes noise suppression increasingly challenging, prompting Würth Elektronik to expand the smallest packages of the STAR-TEC and STAR-TEC LFS families in its ferrite range.

The STAR-TEC snap ferrites are used for retroactive suppression of frequency-dependent and conducted interference on single conductors in the frequency range from 1 MHz to 1 GHz. The STAR-TEC LFS series of snap ferrites were specifically designed for low-frequency applications in the 300 kHz to 30 MHz range.

Only opened with a key

The snap ferrites from Würth Elektronik are distinguished by their outstanding user-friendliness. The cable pre-fixation feature simplifies handling, and the pinching safeguard prevents assembly faults. The key, included with sample deliveries, allows the ferrites to be opened and reinstalled at any time, making EMC testing a snap. The internal lock also prevents unauthorized cable removal without the key.

No additional tools required for attachment

The new snap ferrites, designed specifically for thin cables, offer the crucial advantage of integrated cable fixation, allowing them to be attached without additional tools such as cable ties, heat shrink tubing, or adhesive tape.

The robust and compact plastic housing of the NiZn and MnZn ferrites is classified according to UL94 V0 and specified for an operating temperature range of -50°C to +105°C.

All STAR-TEC and STAR-TEC LFS snap ferrites, now available for cable diameters between 2 and 25 mm, can be ordered from stock with no minimum order quantity. Free samples are available for developers.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in