Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

02. February 2023
Components

High Current Inductor for Automotive Applications

Content you may also like

Bauteil auf weißem Grund

Würth Elektronik presents WE-XHMA SMD Power Inductor

Waldenburg (Germany), February 2, 2023 – Würth Elektronik introduces another AEC-Q200 certified SMD inductor: WE-XHMA features an extremely high current capability of up to 50.6 A saturation current and the ability to handle high current transient peaks. Its design with flat wire coil and a composite core material ensures low copper losses and stable behavior under temperature fluctuations

WE-XHMA is particularly suitable for use in DC/DC converters for high current supply and field programmable gate arrays (FPGA), as well as filter applications. It is particularly useful when used in switching power supplies: In contrast to conventional core materials, the compact coil shows hardly any temperature-dependent fluctuations in terms of inductance and saturation current. The higher energy density and the compact design due to the use of flat wire also make WE-XHMA interesting for switched-mode power supplies. Flat wire also has the advantage that a larger cross-sectional area can be achieved with the same space requirement, thereby reducing resistance. Furthermore, it shows a lower skin effect at higher frequencies and the heat dissipation towards the circuit board is, because of the flat thermally conducting surface, also better than round wire.

The compact molded magnetically shielded coils are AEC-Q200 certified and have an operating temperature range of -40°C to +125°C. WE-XHMA is available from stock in SMT styles 6030, 6060, 8080, 1090, 1510 and with saturation currents from 9.3 to 50.6 A. Free samples for developers are provided.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in