Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

28. May 2024
Components

Eight New Sizes in the Extremely Efficient Inductor Series

Content you may also like

Black WE-XHMI components on a white background

Würth Elektronik expands its range of power inductors

Waldenburg (Germany), May 28, 2024 – In addition to Würth Elektronik’s five existing package sizes of WE-XHMI SMT power inductors there are now eight new packages. These compact yet extremely efficient inductors feature high current capacity up to 56 A saturation current and the ability to handle high transient current spikes. This makes them particularly suitable for use as DC/DC converters in power supplies, point-of-load converters and high-current filters, as well as in industrial computers, mainboards and graphics cards.

The molded flat wire inductor, previously only available in the Power Magnetics product family, now also comes in 4020, 4030, 4040, 5020, 5030, 5050, 7030 and 7070 package sizes.The series is also available in smaller packages, and the 70xx sizes close a gap in the existing portfolio. The new packages help to further optimize the production process, resulting in a significant improvement in the electrical properties RDC, Isat and Ir.

The AEC-Q200-qualified WE-XHMI series inductors can be used at operating temperatures from -40°C to +125°C and cover an inductance range from 0.15 to 33 µH with currents up to 56 A.

Advantage of flat wire coils

Using the WE-XHMI flat wire inductor improves efficiency and effectiveness thanks to very low winding resistance. The design as a flat wire coil with a composite core material achieves extremely low copper losses and stable behavior with temperature fluctuations. What’s more, the use of flat wire reduces the skin effect, as there is a larger surface area with the same cross-section.

All package sizes of SMT power inductors are now available from stock without a minimum order quantity. Free samples are available for developers.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in