Reference project BAUS

Reference project BAUS

Adaptable to standards around the world

B.A.U.S. AT relies on components from Würth Elektronik ICS for ambulances

B.A.U.S. AT, a renowned manufacturer of rescue vehicles, is equipping its ambulances for the international market with power distributors and displays from Würth Elektronik ICS. These components make it possible to optimally meet the different requirements and standards of various countries.

 

The following solutions from Würth Elektronik ICS were used:
 

Power distributor in solid press-fit technology:

  • Mechanically very robust, vibration-resistant and durable
  • Low contact resistance and little heating
  • Easy and quick installation and maintenance
  • Reduced cable harness

 

WEcabin Displays i5

  • For controlling lamps, fans and heating
  • Advanced microprocessor
  • Optional equipment with buttons, Wi-Fi, Bluetooth and sensors possible
  • Fast booting and intuitive operation
  • High connectivity with freely definable CAN communication structure
  • Easy programming without specialist knowledge

 

B.A.U.S. AT plans to further expand its cooperation with Würth Elektronik ICS, particularly in the area of customer-specific power distribution boards. A further development of the power distribution board for the French market is currently being driven forward in close cooperation between the two companies.

 

Extensive test phase

The installed products were tested in the prototype phase according to the following criteria:

•          Electromagnetic compatibility and electrical load according to EMC ISO 13766, ISO 16750-2, ISO 14982

•          Water resistance according to IP66 ISO 20653

•          Salt spray resistance according to ISO 9227

•          Vibration & shock according to ISO 16750-3

•          Chemical resistance according to ISO 16750-5

•          Temperature according to ISO 16750-4

More about the product solutions used

Other successfully implemented projects

  • Two development approaches - two success stories

    Krone, the leading manufacturer of agricultural machinery in Europe, has been relying on the innovative power distribution solutions from Würth Elektronik ICS for over 10 years. 

  • Würth Elektronik ICS equips Komatsu wheel loader

    Komatsu upgraded the user-friendliness and functionality of its products with individually developed solutions from Würth Elektronik ICS. 

  • Smart box for a leaner wiring harness

    Dieci uses the REDline Power Box Hybrid from Würth Elektronik ICS in different versions. Our reference project shows how we individually developed the REDline Power Box Hybrid in three different ways.

  • Compact Electrics for telehandlers

    When the Bobcat telehandlers were completely revised in recent years, the electrical system of the vehicles was also taken into consideration. Würth Elektronik ICS is one of the development partners that supported that improvements. The result is a set of compact fuse and relay boxes that minimize the amount of wiring required.