The Orthosie-I module is based on the ESP32-C3 chipset by Espressif Systems and therefore supported by the esp-project, which allows the module to be used as a WiFi and Bluetooth® LE interface using Raspberry Pi as a host. This application note shows, which parts are applicable and which steps have to be performed to integrate the Orthosie-I module in Raspberry Pi.
Download: ANR035