Radio Module
19. February 2025

Build your own firmware - getting started with Zephyr®

Content you may also like

anr035-orthosie-i-integration-in-raspberry-pi

Zephyr® OS is an operating system for micro-controllers distributed by the Linux® Foundation

and used in many end devices. This operating system includes features like multi-threading

and dynamic memory allocation. It also supports various radio stacks and provides many functions

for using external electronic components, such as sensors, radio modules, and displays.

Besides the radio modules with integrated firmware, Würth Elektronik eiSos also offers various

BYOF (build your own firmware) variants of them. These radio modules come without firmware

and are therefore highly suited to develop optimized custom solutions for special applications.

To be able to use the integrated Zephyr® stacks and features on Würth Elektronik eiSos radio

module hardware, Würth Elektronik eiSos integrated the hardware description of their BYOF

modules into the Zephyr® SDK. With this, the BYOF hardware platform of interest can be

simply selected during firmware development using the Zephyr® SDK.

Download: ANR036

Content you may also like