A common solution to maintain the performance of NFC antennas, is to use high permeability absorber films. However, this can result in resonant frequencies being shifted to lower values. Therefore, in „Design approach for high efficiency NFC systems with magnetic shielding materials” different thicknesses of the same ferrite polymer material are evaluated and the shielding effect between the conductive surface and the NFC antenna is analyzed. This paper was first published at the EMC Europe Conference 2020.
To the technical paper.
Further information on shielding for 5G applications
Continue Reading
Different absorber films are characterized based on the coupling between two antennas
Continue Reading
Various material compositions based on glass fiber in combination with conductive materials are described
Continue Reading