Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

18. February 2025
Components

Automotive Quality up to 250 A

Content you may also like

REDCUBE PRESS-FIT for Automotive: The individually tested press-fit connectors can carry high currents and are mechanically very stable.

PCB threaded connections using press-fit technology

Würth Elektronik, manufacturer of electronic and electromechanical components for the electronics industry, presents its “REDCUBE PRESS-FIT for Automotive”, a new range of threaded connections specially optimized for the automotive industry. The robust components can carry currents of up to 250 A and are manufactured according to particularly stringent quality standards.

The automotive industry includes some of the most demanding customers. Reworked products aren’t acceptable. High requirements apply to the components used, especially for current-carrying connections. They must be mechanically stable, highly conductive, and not thermally stress the circuit board.

Reliable press-fit technology

Würth Elektronik now serves this demanding market with its new screw connectors for circuit board assembly using press-fit technology. The process ensures an even contact between the pin and the copper layer, especially on PCBs with very thick coatings, and offers greater reliability and stability than soldering. The new connectors enable a gas-tight and extremely strong mechanical connection. The contact resistance for the new automotive series is less than 200 µOhm. Three variants are available:

  • WE-PFIFUA with internal thread (Full Plain Automotive)
  • WE-PFEFUA with external thread (Automotive)
  • WE-PFICFA with internal thread (Circumference Automotive)

Each connector is available in the thread sizes M3, M4, M5, M6 and M8.

Visually checked individually

Each and every component is visually inspected for dimensional accuracy during manufacture. The pins are particularly robust to prevent bending during transport or assembly. This ensures consistently high-quality production results. REDCUBE PRESS-FIT connectors made from RoHS-compliant CuZn39Pb3 alloy can be pressed in without thermally stressing the PCB.

The high-quality threaded connections are used wherever large amounts of energy need to be carried safely and with minimal loss, such as in IGBT power modules, inverters for electric vehicles, or charging stations.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in