Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

09. April 2025
Components

More Compact and Heat-Resistant

Content you may also like

1608 package – the reliable and energy-efficient LEDs of the WL-SMTW series with a miniature-format addition.

Würth Elektronik adds to its robust LED family

Würth Elektronik adds to its successful WL-SMTW LED series with two new variants. The SMT-mountable mono-color top-view LEDs are now available in a 1608 package. New LEDs are being added in the standard 3528 package, which feature an increased operating temperature of up to 100°C. The water-clear glass used enables precise color rendering at maximum intensity in five or six different colors.

With dimensions of just 1.6 × 0.8 × 0.55 mm, the new 1608 variant expands the WL-SMTW product line with particularly compact LEDs. These LEDs have proven to be highly reliable and energy-efficient. The miniature components are available in blue, green, yellow, amber, and two shades of red with wavelengths of 630 or 640 nm. Like all LEDs in the series, they emit no UV and IR.

The WE-SMTW 3258 HIGHTA is the third series of LEDs from Würth Elektronik following WL-SMCW 0603 and WL-SMTD that can withstand temperatures up to 100°C. The 3.5 × 2.8 × 1.85 mm LEDs are available in blue, green, yellow, amber, and red.

The application options for the robust and energy-efficient LEDs are wide ranging. They are suitable for signage and indirect lighting, backlighting in telecommunications applications or LCDs, as well as in fiber optic technology, Industrial and medical technology applications. As usual, Würth Elektronik offers all products in the series from stock with no minimum order quantity.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in