Person sitting in front of a laptop with news on the screen

Press

Welcome to the Press Center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

16. October 2024
Components

USB Power According to the EU Standard

Content you may also like

USB socket WR-COM USB 3.1 PD Type C – Power Only SMT

Intelligent power supply and charging interface

Waldenburg (Germany), October 16, 2024 – Just in time for EU interface standardization, Würth Elektronik presents its new USB socket WR-COM USB 3.1 PD Type C – Power Only SMT. Used exclusively for power transmission, it supports the USB Power Delivery (USB-PD) communication protocol for adaptive charging up to 240 W.

By the end of 2024, the proliferation of charger types for small electronic devices will come to an end. The EU is making USB-C connectors and the USB Power Delivery standard mandatory across the board.

The new USB-C socket from Würth Elektronik, designed exclusively as a power supply and charging interface, meets the new standard. It communicates with the power supply and automatically determines the maximum charging power. In EPR (Extended Power Range) mode, up to 240 W flows into the batteries. Intelligent communication ensures particularly short charging times and prevents damage to circuits due to excessive currents.

Robust, easy-to-install design

For mechanically and electrically reliable installation, the six-pin socket is designed as a horizontal receptacle SMT component with six solder pins: four pins for power supply (Vbus and GND) and two for communication to determine the operating voltage (CC). The contacts come with a nickel barrier layer and a flash gold coating. A nickel coating provides the shielding plating (housing) with high corrosion protection. The thermostable LCP (Liquid Crystal Polymer) plastic parts used are suitable for the reflow soldering process. Moreover, the LCP is ideally suited for the high demands of mechanical durability required by the USB standard.

The intelligent USB socket is used wherever the USB interface is used only for power transmission, for example:

  • Industrial PCs and laptops
  • Displays
  • Mobile input devices
  • Handheld controllers
  • Power banks
Share:

Content you may also like

Press Contacts

Do You Have Any Questions, Comments or Requests Regarding Our Press Work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here You Can Download the Press Information and Pictures of the Company Area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Woman leafs through a technical book from Würth Elektronik

    Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Hand points to iPad, which is held by another person

    Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Colleague views components with a magnifying glass

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You Might Also Be Interested in