OverviewAll product unitsProduct unitPassive ComponentsProduct groupCapacitorsProduct familyFilm Capacitors

Würth Elektronik Capacitors

Big Portfolio available ex stock

Würth Elektronik has extended its capacitor portfolio. You will find an overview of our current technologies available ex stock in the graph. More details (e.g. series, characteristics, features, applications, etc.) about each product family can be found in the flyer or for example below. In our flyer you will also find information about our services.

Characteristics

Film capacitors have a good current carrying capacity and are not dependent on voltage, such as MLCCs with DC bias behavior. The ESR value is low, which can be a significant factor in DC link applications compared to electrolytic capacitors, for example. In addition, film capacitors have a good longevity due to their self-healing properties.

Inner Structure

The picture shows the internal structure of our film capacitors using our WCAP-FTX2 (X2-Capacitors) series as an example. Film capacitors consist of a wound metalized plastic film. The pins are attached to this winding and then sealed in a plastic box using epoxy resin.

Measurements

Redexpert

With the help of REDEXPERT you will find the right capacitor based on your technical requirements. The tool supports, for example, with measured values for capacitance, impedance, ESR and dissipation factor (DF). The ability to compare individual components with each other in terms of measured values enables convenient component selection.

Webinar

Introduction to the capacitor technologies and how to use them

Capacitors make up two thirds of all electronic components and there is a huge diversity of technologies which can overwhelm young engineers. All capacitors store electrical energy in the electrical field created in a dielectric material and they are used for very diverse applications like voltage stability and filtering. How that works differs between tiny MLCCs and huge electrolytic cells, from pF ratings up to the hundreds of Farads in supercapacitors. In this presentation, we introduce different capacitor solutions taking into account the advantages and disadvantages and with a focus on the final application.

Webinar: Introduction to the capacitor technologies and how to use them

Applications Notes, Documents and Videos