07. August 2024
Components

One Component, Two Applications

Content you may also like

WE-RFI can be used as an inductor for HF applications or as a ferrite for interference suppression.

Würth Elektronik extends its series of wire-wound ferrites

Waldenburg (Germany), August 7, 2024 – Würth Elektronik now offers its WE-RFI inductors in sizes 0402 and 0603, which can be used as inductors for HF applications or as ferrites for interference suppression. Here the manufacturer responds to increasing miniaturization and complements the existing sizes 0805 and 1008. The components are suitable as low-pass filters (for filtering high-frequency noise), data line filters, supply voltage decoupling, low-frequency radio applications, and RFID.

As wire-wound ferrites, the WE-RFI inductors attain higher impedances than normal ferrites, even at high frequencies, and over a wider bandwidth. Unlike multilayer ferrites, they show no DC bias behavior.

As HF inductors, they offer high inductance values from 20 nH up to 47 µH. They are characterized by low RDC and consequently a high rated current of up to 1.91 A at ΔT = 40 K. A design kit is available for this component group, which Würth Elektronik will always replenish free of charge, so developers always have inductances of different values to hand.

Share:

Content you may also like