On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik expands its range of inductors to include Power Molded Flat-Wire Inductors
Würth Elektronik introduces its new molded flat-wire inductor with the designation WE-PMFI. The compact inductor measures just 2.0 × 1.6 × 1.0 mm in its smallest package. It also impresses with an exceptionally low resistance (RDC from 4.8 mΩ), an operating voltage of up to 48 V, as well as an extended temperature range from -55°C to +150°C, making it particularly suitable for DC/DC converter assemblies in compact applications that require high output currents and switching frequencies exceeding one megahertz.
Flat-wire technology offers a host of advantages for inductors: they are mechanically more robust as well as optimized heat dissipation. The wire shape utilizes the winding area more efficiently, allowing for higher inductance values in the same package size as compared to round wire. Flat-wire windings also offer a larger cross-sectional area, thus reducing resistance and I2R losses. Eddy current losses, especially in high-frequency applications, are also lower in a flat-wire inductor compared to the round-wire version. These properties have enabled Würth Elektronik to develop a new generation of components that are more compact, temperature-resistant, and far more energy-efficient. They open up new design options for developers.
Minimum dimensions, maximum efficiency
This small and highly efficient inductor is ideal for powering CPUs and RAM in portable electronic devices, such as smartphones and tablets. Measurements with comparable components on the market have shown that the WE-PMFI has 50% lower DC resistance, 40% higher rated current, and 30% higher saturation current.
Available from 100 nH to 4.7 µH
The new molded flat-wire inductor is now available in a broad range of inductance values from 100 nH to 4.7 µH. As with all Würth Elektronik components, free laboratory samples of the new flat-wire inductor can also be ordered.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press Information and pictures of the company area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik Blog
Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.