Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

23. April 2025
Components

For High Switching Frequencies and Output Currents

Content you may also like

Very small and efficient: WE-PMFI

Würth Elektronik expands its range of inductors to include Power Molded Flat-Wire Inductors

Würth Elektronik introduces its new molded flat-wire inductor with the designation WE-PMFI. The compact inductor measures just 2.0 × 1.6 × 1.0 mm in its smallest package. It also impresses with an exceptionally low resistance (RDC from 4.8 mΩ), an operating voltage of up to 48 V, as well as an extended temperature range from -55°C to +150°C, making it particularly suitable for DC/DC converter assemblies in compact applications that require high output currents and switching frequencies exceeding one megahertz.

Flat-wire technology offers a host of advantages for inductors: they are mechanically more robust as well as optimized heat dissipation.  The wire shape utilizes the winding area more efficiently, allowing for higher inductance values in the same package size as compared to round wire. Flat-wire windings also offer a larger cross-sectional area, thus reducing resistance and I2R losses. Eddy current losses, especially in high-frequency applications, are also lower in a flat-wire inductor compared to the round-wire version. These properties have enabled Würth Elektronik to develop a new generation of components that are more compact, temperature-resistant, and far more energy-efficient. They open up new design options for developers.

Minimum dimensions, maximum efficiency

This small and highly efficient inductor is ideal for powering CPUs and RAM in portable electronic devices, such as smartphones and tablets. Measurements with comparable components on the market have shown that the WE-PMFI has 50% lower DC resistance, 40% higher rated current, and 30% higher saturation current.

Available from 100 nH to 4.7 µH

The new molded flat-wire inductor is now available in a broad range of inductance values from 100 nH to 4.7 µH. As with all Würth Elektronik components, free laboratory samples of the new flat-wire inductor can also be ordered.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in